AXIS#.MOTOR​.BRAKEPOWERDELAY

Description

Time to wait after applying full voltage before dropping to low voltage when AXIS#.MOTOR​.BRAKEPOWERSAVING = 1.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Milliseconds

Range

0 to 2000

Default Value

150

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.MOTOR.BRAKEPOWERDELAY

500bh

24h

Unsigned16

-

-

Read/Write

No

AXIS2.MOTOR.BRAKEPOWERDELAY

510bh

24h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.BRAKEPOWERDELAY

6238

185E

Unsigned16

Read Only

-

AXIS2.MOTOR.BRAKEPOWERDELAY

71774

1185

Unsigned16

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.BRAKEPOWERDELAY

6238

Unsigned16

Read Only

-